Harmonic Drive aboutusHarmonic Drive ProductsHarmonic Drive ReferenceHarmonic Drive SupportHarmonic Drive Sales ContactsHarmonic Drive Employment Opportunities
PAGE: "Reference | Application Notes | Installation Considerations for Component Sets :: Harmonic Drive LLC"
URL: http://www.harmonicdrive.net/reference/applicationnotes/installcomp.php

Application Notes



Installation Considerations for Component Sets

The following information is directed toward technicians or personnel, who are involved in the assembly or installation of Harmonic Drive™ strain wave gearing.
  1. Refer to recommended housing tolerances and component set drawing for proper installation specifications.
  2. Use the recommended lubricants and proper quantity. Replace the lubricant at the recommended service interval.
  3. There are four areas within the gear that require lubrication.
    • A) Wave Generator Bearing
    • B) Oldham Coupling (if one is included)
    • C) Gear Teeth
    • D) Inner diameter of Flexspline
  4. The Wave Generator must be securely fastened to the input hub to prevent axial movement along the input shaft.
  5. The Wave Generator must be assembled concentrically with the Circular Spline to prevent an improper assembly. Refer to the section named "Dedoidal" in our catalog.
  6. The surface to which the Circular Spline is clamped, must be clean, flat, and free of debris or burrs. Tighten screws using a torque wrench and use no other locking hardware except the suitable grade Loctite sealant or equivalent.
  7. The part numbering method is as follows (space permitting).
    SS XX JJJJJJ Q

    SS: Size
    XX: Ratio
    JJJJJJ: Serial Number
    Q: Set Number

    In order to obtain the published performance specifications, it is essential that the component set remains as a matched set. Each component within the component set must have the same part number, including the set number. The above number may be required for ordering replacement drives.
  8. Proper seals, gaskets, or sealants must be used to contain the small amount of oil that may separate from the grease.
  9. The Component Set has been coated with a rust preventative oil for storage purposes, and must be thoroughly cleaned prior to use.
  10. There are two types of component sets: Cup-Type and Pancake-Type.

The Cup-Type has a Flexspline that is shaped like a cup.

The Pancake-Type has a Flexspline that is a thin sleeve with gearteeth on the outside diameter. The Pancake-Type has an additional item called a Dynamic Spline, which appears to be similar to the Circular Spline. The Dynamic Spline has larger chamfers than the Circular Spline. These two items are not interchangeable.

We encourage you to call us at 800-921-3332 or 978-532-1800 if you have any questions or comments.




[ Harmonic Drive LLC | About Us | Products | Reference | Support | Disclaimer ]
© 2012 Harmonic Drive LLC | 800-921-3332
The World's Largest Manufacturer of Precision Strain Wave Gearing and Motion Control Products
Long Island Web Design